#pragma CREATE_ASM_LISTING: Create an Assembler Include File Listing

Scope

Next pragma CREATE_ASM_LISTING

Syntax
  #pragma CREATE_ASM_LISTING (ON|OFF) 
  
Synonym

None

Arguments

ON: Creates an assembler include file for all subsequent defines or objects

OFF: Does not create an assembler include file for all subsequent defines or objects

Default
  OFF 
  
Description

This pragma controls whether subsequent defines or objects are printed into the assembler include file.

A new file generates only when the -La compiler option is specified together with a header file containing #pragma CREATE_ASM_LISTING ON.

Example
  #pragma CREATE_ASM_LISTING ON

  
  extern int i; /* i is accessible from the asm code    */

  
  #pragma CREATE_ASM_LISTING OFF

  
  extern int j; /* j is only accessible from the C code */

  
See also

-La: Generate Assembler Include File

Generating Assembler Include Files (-La Compiler Option)