Macros for HC08

The following table lists the size_t macro settings for the HC08 target.

Table 1. size_t Macro Settings
size_t Macro Defined
__SIZE_T_IS_UCHAR__ -Mt
__SIZE_T_IS_USHORT__ Never
__SIZE_T_IS_UINT__ -Ms, -Mb
__SIZE_T_IS_ULONG__ Never

The following table lists the ptrdiff_t macro settings for the HC08 target.

Table 2. ptrdiff_t Macro Settings
ptrdiff_t Macro Defined
__PTRDIFF_T_IS_CHAR__ -Mt
__PTRDIFF_T_IS_SHORT__ Never
__PTRDIFF_T_IS_INT__ -Ms
__PTRDIFF_T_IS_LONG__ Never