-H: Short Help

Group

VARIOUS

Scope

None

Syntax
  -H   
Arguments

None

Default

None

Defines

None

Pragmas

None

Description

The -H option causes the Compiler to display a short help list of available options within the Compiler window. Options are grouped into HOST, LANGUAGE, OPTIMIZATIONS, OUTPUT, INPUT, CODE GENERATION, MESSAGES, and VARIOUS.

Do not specify any other option or source file when the invoking -H option.

Example

The following listing shows the short list options.

Listing: Short Help Options
-H may produce the following list:
INPUT:

-!     Filenames are clipped to DOS length

-I     Include file path

VARIOUS:

-H     Prints this list of options

-V     Prints the Compiler version