If you start the compiler with no options and no input files, the tool enters the interactive mode and the compiler GUI is displayed. This is usually the case if you start the compiler using the Windows Explorer or an Desktop or Programs menu icon.
The following code specifies an input line associated with a desktop icon for the HC(S)08 compiler:
chc08.exe -F2 a.c d.c