Help Menu

Use the Help menu to activate or deactivate the Tip of the Day dialog box at application startup. In addition, it provides access a standard Windows Help file and an About box. The table below lists the Help menu options.

Figure 1. Help Menu

Help Menu

Table 1. Help Menu Options
Menu Option Description
Tip of the Day Activates or deactivates Tip of the Day at startup.
Help Topics Standard Help topics.
About Displays an About dialog box with version and licensing information.