Open the Environment Configuration dialog box to configure the environment. The dialog box's content is read from the [ Environment Variables] section of the actual project file.
The following listing shows the available environment variables.
General Path: GENPATH Object Path: OBJPATH Text Path: TEXTPATH Absolute Path: ABSPATH Header File Path: LIBPATH Various Environment Variables: other variables not mentioned above.
The following buttons are available in this dialog box.
| Button | Function |
|---|---|
| Add | Adds a new line or entry |
| Change | Changes a line or entry |
| Delete | Deletes a line or entry |
| Up | Moves a line or entry up |
| Down | Moves a line or entry down |