Selecting this editor option, as shown in the figure below, associates a separate editor for error feedback with the application. The configured editor (that is, Global or Local) is not used for error feedback.
In the Command Line text box, enter the command that starts the editor.
The format of the editor command depends on the syntax. Specify Modifiers in the editor command line to refer to specific line numbers in the file. (Refer Modifiers.)
The format of the editor command depends upon the syntax that is used to start the editor.