You can use the HC(S)08 Compiler as a standalone compiler. In this section, we will create a new project directory using some of the previously created files, and build the application.
Note:
Although it is possible to create and configure a project from scratch using the standalone Build Tools, it is easier and faster to create, configure, and manage your project using the CodeWarrior Projects wizard.