Selecting Input Files

The project does not contain any source code files at this point. Copy and paste the C source code (*.c) and header (*.h) files from the previous project, HCS08_project, to save time.

  1. Copy the Sources folder from the HCS08_project folder and paste it into the X15 project folder.
  2. Copy the Project_Headers folder from the HCS08_project folder and paste it into the X15 project folder.
  3. Copy and paste the HCS08_project project's Lib folder into the X15 project folder.
  4. In the X15 folder, create a new folder Project_Settings. Copy and paste the Startup_Code folder from the HCS08_project\Project_Settings folder into the X15\Project_Settings folder.

Now there are five items in the X15 project folder, as shown in the figure below: