Use this panel to optimize the library functions for the HC(S)08 compiler.
The following figure shows the
Optimize Library Function panel.
Figure 1.
Tool Settings - HCS08 Compiler > Optimization > Optimize Library Function

Note:
For information about the description of the options appearing in the
Optimize Library Function
panel for HC(S)08 compiler, refer to the
-Oilib: Optimize Library Functions topic.