HCS08 Compiler > Language > CompactC++ features

Use this panel to specify the options to disable the CompactC++ features for the HC(S)08 Compiler. The following figure shows the CompactC++ features panel.

Figure 1. Tool Settings - HCS08 Compiler > Language > CompactC++ Features

Tool Settings - HCS08 Compiler > Language > CompactC++ Features

Note: For information about the description of the options appearing in the CompactC++ features panel for HC(S)08 Compiler, refer to the