The following sections describe the settings panels that configure the HC(S)08 Compiler build tool options. These panels are part of the project's build properties settings, which are managed in the
Properties
window. To access these panels, proceed as follows:
- Select the project for which you want to set the build properties, in the CodeWarrior Projects view.
- Select Project > Properties from the IDE menu bar.
The
Properties for <project>
dialog box appears.
- Expand the C/C++ Build tree control and select Settings.
The various settings for the build tools are displayed in the right panel. If not, select the
Tool Settings
tab.
The options are grouped by tool, such as
Messages
,
Host
,
General
,
Disassembler
,
Linker
,
Burner
,
HCS08Compiler
,
HCS08 Assembler
and
Preprocessor
options. Depending on the build properties you wish to configure, select the appropriate option in the
Tool Settings
tab page.
Note: For information about other build properties panels, refer to the Microcontrollers V10.x Targeting Manual.
The following listed are the build properties panels for the HC(S)08 Compiler.