HCS08 Compiler

Use this panel to specify the command, options, and expert settings for the HC(S)08 compiler. Additionally, the HCS08 Compiler tree control includes the general, include file search path settings. The following figure shows the HC(S)08 Compiler settings.

Figure 1. Tool Settings - HCS08 Compiler

Tool Settings - HCS08 Compiler

The following table lists the HSC08 Compiler panel options for HC(S)08 Compiler.

Table 1. Tool Settings - HCS08 Compiler Options
Option Description
Command Shows the location of the linker executable file. Default value is: "${HC08Tools}/chc08"
All options Shows the actual command line the compiler will be called with.
Expert Settings

Command line pattern

Shows the expert settings command line parameters; default is ${COMMAND} ${FLAGS}${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT}${INPUTS}