Introduction

This chapter describes the HC(S)08 Compiler that is part of the CodeWarrior Development Studio for Microcontrollers V10.x. The Compiler consists of a Frontend, which is language-dependent, and a Backend, which is hardware-dependent and generates object code specific to HC08 and HCS08. Chapters one and two describe the configuration and creation of projects that target HC08 and HCS08 microcontrollers. Chapter three describes the Compiler in greater detail.

Note: The CodeWarrior Development Studio tools actually support both the HC08 and HCS08 Microcontroller derivatives. For brevity, this document uses the label HC(S)08 to describe where the tools support both Microcontrollers derivatives. Where information is specific to HC08, the label HC08 is used, and where it is specific to HCS08, the label HCS08 is used.

This chapter consists of the following topics.