Changing Class Associated with Message

Use the buttons located on the right hand side of the panel to configure your own message mapping among the different message classes. Each button refers to a message class. To change the class associated with a message, select the message in the list box and then click the button associated with the class to which you want to move the message.

To define a warning message as an error message:

  1. Click the Warning panel to display the list of all warning messages in the list box.
  2. Select the message you want to change in the list box.
  3. Click Error to define this message as an error message.
    Note: Messages cannot be moved to or from the fatal error class.
    Note: The Move to buttons are active only when messages that can be moved are selected. When you select a message which cannot be moved to a specific group, the corresponding Move to button for that group is disabled (grayed).

To save your changes to the message mappings, click OK to close the Message Settings panel. Clicking Cancel discards your changes and closes the panel.