Parameters available for RTOS functions

The current RTOS functions permit entering a variety of parameters to complete the function call. These available values are internal symbols of macrolanguage (the internal language of Processor Expert). It is important to select the correct symbols for the correct functions so that Processor Expert is capable of producing the correct C code for the LDD.

The values are the following:

For more information and to understand the usage of these values, refer to the Creating RTOS component topic.