Timeline

The timeline data displays the functions that are executed in the application and the number of cycles each function takes when the application is run.

To view timeline data:

  1. In the Software Analysis view, expand the project name.

    The data source is listed under the project name.

  2. Click the Timeline hyperlink.

    The Timeline viewer appears.

    Figure 1. Timeline Viewer Displaying Timeline Data
    TraceTimelineEditor Viewer Displaying Timeline Data

The Timeline viewer shows a timeline graph in which the functions appear on y-axis and the number of cycles appear on x-axis. The green-colored bars show the time and cycles that the function takes. The gray-colored bar represents the Low Power WAIT Mode of the application.

The TraceTimelineEditor viewer also displays the following buttons: