Viewing Data

You can view the collected data for various targets such as HCS08, ColdFire V1, Kinetis, MPC56xx and DSC from the data file generated after running the application in the following viewers.

You can also view trace data of the other project by importing the trace data file of another project into your project using the Import wizard. For more information, refer Importing Trace Data Offline.

Note: This chapter demonstrates how to view collected data on the Kinetis target. The process of viewing data for all the targets is same.