Trace Modes

The triggers can be set in the following trace modes:

Note: The HCS08 target does not generate trace data on the default stationery project. This is because the default source code does not contain any branch required for an HCS08 application to generate trace. To generate trace, you need to add a subroutine to the default code and call it from the main() function.

This topic contains the following sub-topics: