The ColdFire V2 - V4 targets collect the profiling information by using the profiling system. These targets do not have the hardware capability to collect trace. The profiling system consists of three main components:
The profiling system collects information using a profiler, which analyzes the amount of time a program spends performing various tasks and detects bottlenecks between the functions/routines. This type of information-tracking can be useful for determining the cost of calling a routine. The cost of a routine call is not only the time spent in the routine, it is also the time spent in its children, that is the subsidiary routines it calls, the routines they call, and so on.
To use the profiler for profiling an application, perform the following actions:
This process of profiling gets you all the data you need to perform a professional-level analysis of the runtime behavior of your application.
This chapter contains the following topics: