Getting Started

The CodeWarrior Profiling and Analysis tool lets you collect data of an application. You can analyze this data to identify the bottlenecks, such as slow execution of routines or heavily-used routines within the application. This chapter explains features of the CW Profiling and Analysis tool, the CW interface that this tool uses, and the type of data that is collected using the tool.

Refer to the following topics: