The Select Working Set dialog box appears.
The New Working Set dialog box appears.

To group tracepoints by working sets, click the drop-down in the Analysispoints view, and select Group By > AnalysispointWorking Sets. The tracepoints grouped by the working sets appear in the Analysispoints view.

You can also set a working set as the default one so that whenever you add any stop or start tracepoint to your application, it gets automatically added to the default working set. In this way, working sets help you work on a particular set of tracepoints at a particular time. Click the drop-down in the Analysispoints view and select the Select Default Working Set option. It opens the Select Default Working Set dialog box where you can set one of the available tracepoints working sets as the default one. Alternatively, right-click the working set, and select the ToggleDefault.label option from the context menu to set the working set as default.
You can deselect the working set which you set as default, using the Deselect Default Working Set option from the drop-down or selecting the ToggleDefault.label option from the context menu.