To configure the launch configuration for the MPC56xx target:
- In the CodeWarrior Projects view, right-click the project and select Debug As > Debug Configurations from the context menu.
The
Debug Configurations
dialog box appears.
- In the Debug Configurations dialog box, expand the CodeWarrior Download configuration in the tree structure on the left, and select the launch configuration corresponding to the project you are using. For example, select MPC5675K_RAM_PnE USB-ML-PPCNEXUS.
To configure the launch configuration for the measurement of data:
- Click the Trace and Profile tab.
- Check the Enable Trace and Profile checkbox.
This configures the launch configuration for the MPC56xx target.
Note: Tracing is not supported for MPC56xx processors with z0 core as these processors do not have a trace buffer.