Prints to the standard output C/C++ managed build, launch configuration or RSE system settings.
ecd.exe -getOptions -project path [-config name | -allConfigs] [- file path] [-option option-name] [-launchConfig name | - allLaunchConfigs] [-rseSystem name | -allRseSystems]
Parameters
-config
The build configuration name. If the -config flag isn't specified, the default build configuration is used.
-allConfigs
Specifies that all build configurations will be edited or listed
-file
The file path of a file included in the project. If the -file flag is specified, a file-level setting is retrieved instead of a build configuration level setting(s). The -file flag does not apply to the -launchConfig , -allLaunchConfigs and -rseSystem flags.
-option
If the option setting isn't specified, all options are printed in a key=value format instead of a single option value, which could be used for discovering the list of option ids in a given build configuration, launch configuration or RSE system.
-option-name
Specify the option name.
-launchConfig
The launch configuration name. Allows retrieving launch configuration settings.
-allLaunchConfigs
Allow retrieving all launch configuration settings.
-rseSystem
The RSE system name. Allow retrieving RSE system settings.
-allRseSystems
Lets you retrieve RSE targets and connections settings.