Builds a set of C/C++ projects. Multiple-project flags can be passed on the same command invocation. The build tool output is generated on the command line, and the build result is returned by ecd.exe return code, as 0 for success, and -1 for failure.
ecd.exe -build [-verbose] [-cleanAll] [ -project path [ - config name | -allConfigs] -cleanBuild]
-cleanBuild
The -cleanBuild command applies to the preceding -project only.
-cleanAll
The -cleanAll command applies to all -project flags.
-config
The build configuration name. If the -config flag isn't specified, the default build configuration is used.