Target Processor Selection

The target process selection combo box enables you to refine the list of target processors in the combo box. When you start entering text in the combo box text field, with every character you type, the choices are reduced to ones which contains the sequence of characters typed in the text field.




This Information Center content is based on CWCFUG Rev 10.5, 09/2013, which can be downloaded from www.freescale.com.