Remote System Changed dialog

The Remote System Changed dialog appears when a project is open in the workspace and its APSC cache contains Remote Systems that have different settings to the ones in the existing Remote System tree. In such case, you will be asked to update, discard or create a new set of objects for the cached Remote System settings.

The Remote System Changed dialog provides following three options to resolve the version differences:

  1. Replace the current version with the project version.
  2. Discard the project version and update the project to use the current version.
  3. Create a new Remote System for the project version.
  4. Choose an appropriate option and click OK.

You can click the Configure Project Cache Settings link to directly change the Remote System Project Cache preferences, to avoid automatically displaying this dialog in future. For details, see Remote system project cache preferences.

Note: You may keep the file containing the referenced remote systems available in the <Project_name>/Referenced Systems folder in a version control system for future use.