The
Find and Open File dialog lets you open a selected path or file in the
Editor area.
To open particular path or file in the Editor area:
- Choose File > Open Path from the IDE menu bar.
The
Find and Open File dialog appears.
Figure 1. Find and Open File dialog
- Enter a file descriptor. The file descriptor can be a simple file name, a partial path or a full path. The path delimiters can also be different from that of the native platform delimiters. For example, you can use "/" on a Windows host instead of "\".
- Click OK.
Eclipse IDE performs the following actions: