Displaying referenced projects in CodeWarrior Projects view

The CodeWarrior Projects view displays the referenced projects and highlights which build configuration is referenced.

The following figure shows the Referenced Project in the CodeWarrior Projects view.

Figure 1. CodeWarrior Projects view > Referenced project

CodeWarrior Projects View > Referenced Project

Note: All the project references appear under a Referenced Projects folder, which only shows if the project contains at least one referenced project.

The following table shows the shortcut menu commands available through the CodeWarrior Projects view:

Table 1. Referenced projects - Shortcut menu commands
Command Description
Include in Build It allows you to quickly toggle whether all referenced projects and build configurations will be included in the build or not.
Open/Import Project It is available when the referenced project element is selected and is either closed or does not exist in the workspace. The action imports and/or opens the referenced project in the workspace.
Close Project It is available when the referenced project element is selected and is opened in the workspace. It allows you to close the referenced project in the workspace.
Edit Location Allows you to edit the location of the referenced project.
Remove Referenced Project Allows you to delete the referenced project.