You can create a target configuration for a target running the TRK debug agent.
Note: This feature is not available in StarCore.
To create a TRK target configuration:
- Click File > New > Other.
The
New wizard appears.
- Choose Connection under the Remote System Explorer category.
- Click Next.
The
Select Remote System Type page appears.
- Choose CodeWarrior Bareboard Debugging > TRK Target.
The
TRK Target page appears.
- Choose a parent profile from the Parent profile pop-up menu.
- Type a configuration name in the Name textbox.
- Type connection description in the Description textbox.
- Choose a remote system template from the Template pop-up menu. The remote system template is a pre-defined configuration fully supported by CodeWarrior debugger.
- Choose None from the Template pop-up menu when the current remote system configuration does not use any reference template.
- Click Apply Defaults to load settings from reference template in the current configuration.
- Choose a target type from the Target type pop-up menu or click Edit to import the target type.
- Click the Initialization tab and specify the initialization settings to suit your needs.
- Click the Memory tab and specify the memory configuration settings to suit your needs.
- Click Finish.
The TRK target configuration appears in the
Remote Systems view.