Creating hardware or simulator connection configuration

A hardware or simulator connection configuration helps you create a connection configuration for a hardware-based or simulated target. To create a hardware or simulator connection configuration:

  1. Click File > New > Other.

    The New wizard appears.

  2. Choose Remote System Explorer > Connection.
  3. Click Next.

    The New Connection page appears.

  4. Choose CodeWarrior Bareboard Debugging > Hardware or Simulator Connection.

    The New Connection - Hardware or Simulator Connection page appears.

    Figure 1. New Connection - Hardware or Simulator Connection page

    New Connection - Hardware or Simulator Connection Configuration

  5. Choose a parent profile from the Parent Profile pop-up menu.
  6. Type a configuration name in the Name textbox.
  7. Type connection description in the Description textbox.
  8. Choose a remote system template from the Template pop-up menu. The remote system template is a predefined configuration fully supported by CodeWarrior debugger.
  9. Choose None from the Template pop-up menu when the current remote system configuration does not use any reference template.
  10. Click Apply Defaults to load settings from reference template in the current configuration.
  11. Choose a target from the Target pop-up menu.

    A target type is a CodeWarrior abstraction that represents the users target processor layout. This can be a simple processor or a set of processors as defined by a JTAG configuration file or a Power Architecture® device tree blob file.

  12. Click Edit to add or remove target types.
  13. Click New to create a new target configuration.
  14. Choose a connection type from the Connection type pop-up menu.
    • Choose CCSSIM2 ISS to specify setting for CodeWarrior Connection Server (CCS).
    • Choose Ethernet TAP to specify settings for ethernet TAP connection.
    • Choose USB TAP to specify settings for USB TAP connection.
  15. Click Finish.

    The hardware or simulator connection configuration appears in the Remote Systems view.