Changes to a different directory or lists the current directory. Pressing the Tab key completes the directory name automatically.
Directory pathname; accepts asterisks and wildcards.
The following table lists and defines examples of the cd command.
Table 1. cd Command-line debugger command - Examples| Command |
Description |
| cd |
Displays current directory. |
| cd c: |
Changes to the C: drive root directory. |
| cd d:/mw/0622/ test |
Changes to the specified D: drive directory |
| cd c:p*s |
Changes to any C: drive directory whose name starts with p and ends with s. |