Saving generated assembly code

The generated Assembly (ASM) code is unique for different targets. Follow these steps to save the ASM code generated by the MMU Configuration File Editor:

  1. From the CodeWarrior IDE menu bar, choose MMU Editor > Save ASM to save the generated Assembly code. Alternatively, click the corresponding toolbar buttons in the MMU Configurator toolbar.

    A standard Save dialog appears.

  2. Specify the name of the file in the File name textbox and click Save to save the generated code as a new file.
    Note: The MMU Configuration File Editor regenerates the Assembly code when you change settings in the configuration pages or when you click Change on the Program MATT or Data MATT pages.