The
Register Details view (
Figure 1) shows detailed information for a selected register. The
Register Details pane shows the following information for a register:
- Bit Fields - Shows a graphical representation of the selected register's bit values. This graphical representation shows how the register organizes bits. You can use this representation to select and change the register's bit values. Hover the cursor over each part of the graphical representation to see additional information.
- Actions - Enables you to perform various operations on the selected register's bit-field values.
- Description - Shows explanatory information for the selected register. The information includes name, current value, description, and bit-field explanations and values of the selected register.
Note: The default display of the
Registers view shows register details, such as
Bit Fields ,
Description , and
Actions . To see more register contents, use Registers view pull-down to select
Layout > Registers View Only . To restore the register details, use the view's toolbar menu to select a different menu command.
To open the Register Details view, right-click on a register name in the
Registers view and select
Show Details As > Register Details pane from the context menu that appears . You can also click the
Register Details button on the toolbar to open the
Register Details view.
Figure 1. Register Details View
Note: If the
Registers view loses focus, all pending changes are discarded. For more information, see the <Product> Targeting Manual.
Following sections will help you with more details on the
Register Details view: