Programming a file

  1. Click the Flash Programmer button on the IDE toolbar.

    The Flash File to Target dialog appears.

  2. Choose a connection from the Connection pop-up menu.
    Note: If a connection is already established with the target, this control is disabled.

    The Flash Configuration File pop-up menu is updated with the supported configurations for the processor from the launch configuration.

  3. Choose a flash configuration from the Flash Configuration File pop-up menu.
  4. Select the Unprotect flash memory before erase checkbox to unprotect flash memory before erasing the flash device.
  5. Type the file name in the File textbox. You can use the Workspace, File System, or Variables buttons to select the desired file.
  6. Type the offset location in the Offset textbox.
  7. Click the Erase and Program button.