OS application

OS Application debugging happens through a connection with an agent running on the OS. The connection to the agent is through TCP/IP or COM port. In this scenario, the agent does not have information about the core it is running on, nor does the user specify it when configuring the launch. The user simply specifies the IP address or COM port where the agent is running.

The System Browser view shows the IP address or COM port in the context label.

Figure 1. System Browser view - OS application

System Browser View - OS Application