Multicore Groups

The multicore grouping feature helps you define multiple arbitrary groupings of cores and then perform multicore operations on the groups. Clicking the Multicore Groups button in the Debug view toolbar allows you to create new multicore groups, see Creating multicore group. For more information on multicore debugging, see Multicore debugging.

Figure 1. Multicore Groups

Multicore Groups

The Multicore Groups pop-up menu provides the following options:

The Multicore Groups pop-up menu also shows the list of groups that are shown in the Multicore Groups dialog.