Multicore debugging

The debugger allows simultaneous debugging of multiple projects. This feature provides multi-core debugging capability for some embedded processors. By configuring each project to operate on a single core, the debugger can debug multiple cores by debugging multiple projects.

Note: CodeWarrior for Microcontrollers v10.x does not support debugging multiple projects on multiple cores in the same multi-core target. CodeWarrior for Microcontrollers v10.x supports creating and/or debugging Single Multi Processing (SMP) projects.

Configuring multi-core debugging involves these tasks:

You can use either the user interface or the Debugger Shell to perform multicore operations. In the user interface, you can access multicore operations from these locations in the Debug perspective: