Memory test use cases

The memory read /write and scope loop tests are host based tests. The host machine issues read and write action to the memory through the connection protocol. For example CCS.

Memory tests are the complex tests that can be executed in two modes: Host based and Target based depending upon the selection made for Use Target CPU checkbox.

The Host Based tests are slower than the Target Based tests.