Erasing flash device

To erase a flash device, follow these steps:

  1. Click the Flash Programmer button on the IDE toolbar.

    The Flash File to Target dialog appears.

  2. Choose a connection from the Connection pop-up menu.
    Note: If a connection is already established with the target, this control is disabled.

    The Flash Configuration File pop-up menu is updated with the supported configurations for the processor from the launch configuration.

  3. Choose a flash configuration from the Flash Configuration File pop-up menu.
  4. Select the Unprotect flash memory before erase checkbox to unprotect flash memory before erasing the flash device.
  5. Click the Erase Whole Device button.