Editing multicore group

You can add custom target types by importing files from:

To add and remove system types from multicore groups:

  1. Choose Edit Target Type from the Multicore Groups pop-up menu.

    The Target Types dialog appears.

    Figure 1. Target Types dialog

    Target Types dialog

    • Import - Creates a custom target type by importing it from a configuration file.
    • Remove - Removes a target type from the list.
    • Remove All - Removes all target types from the list.
  2. Click Import.

    The Open dialog appears.

    Figure 2. Import target type

    Import Target Type

  3. Select a multicore configuration file and click Open.

    The multicore appears in the Target Types dialog.

    Figure 3. Added target types

    Added Target Types

  4. Click OK.