Click the Disconnect button in the Debug view toolbar to disconnect a core from the target.
The effect of the disconnect command is same as of the terminate command. The only difference between the two commands is that the disconnect command turns on when a debug session is running.