To use the MMU configurator, you must create an MMU configuration. To create the configuration:
- From the main menu bar, choose File > New > Other.
The New wizard appears.
Figure 1. New wizard - MMU configuration
- Choose Peripheral Configurators > MMU Configuration File.
- Click Next.
The
MMU Configurator File page appears.
Figure 2. MMU Configurator File page
- Enter in the Container textbox the path to the directory in which you want to store the MMU configuration. Alternatively, click Browse and use the resulting dialog to specify the directory.
- Enter in the File name textbox a name for the MMU configuration. Alternatively, leave the default name intact.
Note: If you enter a new name, make sure to preserve the .mmu filename extension.
- Expand Device Number, and select the target hardware for which you are creating the MMU configuration. ( SC3x50)
- Click Finish.
The IDE generates the MMU configuration file in the specified container directory and opens the
MMU Configuration File Editor view.
Figure 3. MMU Configuration File Editor view