Use the
Import/Export/Fill Memory utility to perform various tasks on memory. The utility can be accessed from the
Target Tasks view.
To open the
Target Tasks view:
- Choose Window > Show View > Other from the IDE menu bar.
The
Show View dialog appears.
- Expand the Debug group.
- Select Target Tasks.
- Click OK.
The first time it opens, the
Target Tasks view contains no tasks. You must create a task to use the
Import/Export/Fill Memory utility.
To create a task:
- Click the Create a new Target Task button on the toolbar of the Target Tasks view. Alternatively, right-click the left-hand list of tasks and choose New Task from the shortcut menu that appears.
The
Create a New Target Task page appears.
Figure 1. Create New Target Task Window
- In the Task Name textbox, enter a name for the new task.
- Use the Run Configuration pop-up menu to specify the configuration that the task launches and uses to connect to the target.
Note: If the task does not successfully launch the configuration that you specify, the Execute button of the Target Tasks view toolbar stays unavailable.
- Use the Task Type pop-up menu to specify Import/Export/Fill Memory.
- Click Finish.
The
Import/Export/Fill Memory target task is created and it appears in the Import/Export/Fill Memory Action editor.
Figure 2. Import/Export Memory Action editor