A CodeWarrior project can have multiple associated launch configurations. A launch configuration is a named collection of settings that the CodeWarrior tools use. For example, the project you created in the tutorial chapter had two associated launch configurations.
The CodeWarrior project wizard generates launch configurations with names that follow the pattern projectname - configtype - targettype, where:
Launch configurations for debugging code lets you specify settings such as:
If you use the CodeWarrior wizard to create a new project, the IDE creates two debugger related launch configurations: