Adding breakpoint action

To add a breakpoint action:

  1. Open the Breakpoint Actions preferences page.
  2. Click New.

    The New Breakpoint Action dialog appears.

    Figure 1. New Breakpoint Action dialog

    New Breakpoint Action dialog

  3. In the Action name textbox, enter a name for the new action.
  4. Use the Action type pop-up menu to choose the type of action you want to create.
  5. Specify additional breakpoint-action properties, according to the action type that you specified.

    For example, to display a specified log message when the debugger encounters a breakpoint, specify the log message in the Log Action breakpoint action.

  6. Click OK.

The New Breakpoint Action dialog closes. The new breakpoint action appears in the Breakpoint Actions preferences page table.