Add flash device

To add a flash device to the Flash Devices table:

  1. Click the Add Device button.

    The Add Device dialog appears.

  2. Select a flash device from the device list.
  3. Click the Add Device button.

    The flash device is added to the Flash Devices table in the Flash Programmer Task editor window.

    Note: You can select multiple flash devices to add to the Flash Devices table. To select multiple devices, hold down the Control key while selecting the devices.
  4. Click Done.

    The Add Device dialog closes and the flash device appears in the Flash Devices table in the Flash Programmer Task editor window.

    Note: For NOR flashes, the base address indicates the location where the flash is mapped in the memory. For SPI and NAND flashes, the base address is usually 0x0.