The Memory view lets you monitor and modify your process memory. The process memory is presented as a list called memory monitors. Each monitor represents a section of memory specified by its location called base address. Each memory monitor can be displayed in different predefined data formats known as memory renderings.
The debugger supports the following rendering types:
The default rendering is displayed automatically when a monitor is created.
The Memory view contains these two panes:
The content of the Renderings pane is controlled by the selection in the Monitors pane. The Renderings pane can be configured to display two renderings simultaneously.