Path mappings

The Path Mapping settings are used in IDE to resolve a partial or absolute path from a binary executable during debugging to effectively locate a source file. A binary executable used for debugging typically contains a list of source files in its debugger that were used to build the executable. The source file list is used by the debugger to provide source level debugging. The CodeWarrior IDE supports automatic as well as manual path mapping.

In this section: