seekpos

To alter an input or output stream position.

  virtual pos_type seekpos(
  pos_type sp,

  ios_base::openmode 
     which = ios_base::in | ios_base::out);  
Remarks

The function seekpos() is overridden in strstream classes.

Returns new stream position if successful. Otherwise, it returns pos_type(off_type(-1)).